Lpc11c14 can acceptance filtering (AF)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Lpc11c14 can acceptance filtering (AF)

831件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brecco on Wed Feb 02 04:42:19 MST 2011
good morning,
I need Lpc11c14 can bus sample code for acceptance filtering (AF), Standard Frame Format (SSF) and Extended Frame Format (EFF).
Any ideas...:confused:
Thanks
Louis
0 件の賞賛
返信
2 返答(返信)

810件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by brecco on Wed Feb 02 16:40:43 MST 2011
Zero, thanks for your support.:)
I had already seen your thread.
To start is ok, I have already done the tests on the can bus.
The lpc1768 has examples for acceptance filtering (AF) with Standard Frame Format (SSF) and Extended Frame Format (EFF).
On the contrary, I found no examples of ACCEPTANCE FILTERING for Lpc11c14.:(
Thanks
Louis
0 件の賞賛
返信

810件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Feb 02 06:58:04 MST 2011
Start with:

http://knowledgebase.nxp.com/showthread.php?t=726
0 件の賞賛
返信