Content originally posted in LPCWare by OXO on Thu Feb 02 02:00:32 MST 2012
I have too much to do and I need a small project doing. It's an add-on to a much bigger proj.
I have a 1765 based module which has a USBMSD code, and works fine.
I need to add a HID device and make this into a composite USB device. I also need a small windows app which will talk to the HID and allow display and setting of parameters. The windows app will be a dialog app.
If you are in europe I can supply a board to run the code on, otherwise, maybe you could do it with a lpcxpresso board.
I will be paying for this work..
email me..
spiritsail at the hot mail dot com
Chris