Looking for digital filter example project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Looking for digital filter example project

720件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xjx on Sun Dec 06 13:29:09 MST 2015
Hello,

I am trying to find an example project where CMSIS DSP library is being used.


Only as an example, an application where arm_fir_q31.c file is used would be appreciated. Here I copy the FIR filter function:

  /**
   * @brief Processing function for the Q31 FIR filter.
   * @param[in] *S points to an instance of the Q31 FIR filter structure.
   * @param[in] *pSrc points to the block of input data.
   * @param[out] *pDst points to the block of output data.
   * @param[in] blockSize number of samples to process.
   * @return none.
   */
  void arm_fir_q31(
  const arm_fir_instance_q31 * S,
  q31_t * pSrc,
  q31_t * pDst,
  uint32_t blockSize);

thanks
0 件の賞賛
返信
1 返信

622件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mysepp on Sun Dec 06 13:33:34 MST 2015
Perhaps this page helps:
https://community.freescale.com/thread/357289
0 件の賞賛
返信