Linux - no emulator or board available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux - no emulator or board available

968 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by nbaer89 on Sun Oct 30 17:21:35 MST 2011
I am trying to get my lpc1769 to work on Archlinux, I know its not officially supported but the ide loads fine. The problem I am running into is I cannot debug the board, when I try to run debug I get an error saying there is no emulator or board available.

Is there a workaround for this? Or am I out of luck until I get back to my windows pc?
0 Kudos
Reply
3 Replies

959 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Oct 31 03:27:21 MST 2011

Quote: raghavendrabsrg
Well, This same exact thing is happening to me in my Windows XP 2. with the same error. I think that drivers in my OS is corrupt.. I think the same might be happening to you.. Your linux may not be detecting the hardware attached.



Firstly, take a look at this FAQ (plus the others that it points to, )....
http://support.code-red-tech.com/Cod...ailedToConnect

If you are still having problems, then please answer/try out the following....

Are you running the OS natively or under a virtual machine?
Is this a desktop or a laptop?

Unplug and then reconnect the LPCXpresso board.
- Can you now see the "USB Device with DFU Capabilities" in Device manager?

Can you try connecting using a different USB cable - does this help?
Can you try connecting to a different USB port on your PC - does this help?

If you are still not able to connect, then please run through the diagnostics script below and post the results....
http://support.code-red-tech.com/Cod...inkDiagnostics

Regards,
CodeRedSupport
0 Kudos
Reply

959 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Oct 31 03:26:02 MST 2011

Quote: nbaer89
I am trying to get my lpc1769 to work on Archlinux, I know its not officially supported but the ide loads fine. The problem I am running into is I cannot debug the board, when I try to run debug I get an error saying there is no emulator or board available.


As you recognise, this is not a supported OS.  It might be worth doing a search of previous threads though for "no emulator or board", to see if you can pick up any hints of things to try, for example:

http://knowledgebase.nxp.com/showthread.php?t=2189

Regard,
CodeRedSupport.
0 Kudos
Reply

959 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by raghavendrabsrg on Mon Oct 31 02:50:18 MST 2011

Quote: nbaer89

Is there a workaround for this? Or am I out of luck until I get back to my windows pc?



Well, This same exact thing is happening to me in my Windows XP 2. with the same error. I think that drivers in my OS is corrupt.. I think the same might be happening to you.. Your linux may not be detecting the hardware attached.

In the documentation they've said that IDE supports UBUNTU. so I'm trying that tomorrow.. :)
0 Kudos
Reply