Linux: Building _NXP_LPC176x_Examples_Keil_MCB1700 example projects

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux: Building _NXP_LPC176x_Examples_Keil_MCB1700 example projects

564件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jdsotack on Sun Nov 27 19:13:09 MST 2011
The source files in the _NXP_LPC176x_Examples_Keil_MCB1700 example project in some cases do not use the correct case for the include file names.  Linux, matches case for file names.  If you are getting file not found errors for certain header files with the Linux version of LPCXpresso, you may be able to find them using "locate -i name_of_include_file".

After correcting the case of the #include directives to be consistent with the actual file names, all projects in the workspace built.

John
0 件の賞賛
返信
0 返答(返信)