Linker Config File Rename Bug - V7.7.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linker Config File Rename Bug - V7.7.2

772件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by emh203 on Mon Jul 06 16:55:38 MST 2015
I have an application where I need to manually specify the linker script file name for a project.   I cannot use the managed linker script as it does not appear the "MCU Settings"  dialog is subject to different eclipse build configurations.

I have 2 different build configurations.    One build configuration has a modified linker script to put the start of the application at 0x1A20000.   I have a custom bootloader that exists at 0x1A000000.

So...  When I select a build configuration and go to "Settings-->MCU Linker-->Managed Linker Script" and uncheck the "Manage Linker Script",    the text box for "Linker Script" is changed to PROJECT_NAME.ld  (where PROJECT_NAME is the eclipse project name).

If I try to change the text box,   it will revert to PROJECT_NAME.ld.

Example.

Let's say it starts at "TM4.LD".

I want to change to "TM4_BOOTABLE.ld".

When I click apply it will revert back to "TM4.ld".

Weird part....

if I change to "TM4.bootable.ld", it will accept my change.


Weird bug....

0 件の賞賛
返信
1 返信

756件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jul 07 03:17:43 MST 2015
Thanks for reporting this issue.

It will be fixed in the next release.
0 件の賞賛
返信