License missing when accessing debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

License missing when accessing debug

1,148件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jespern on Mon Dec 27 01:50:58 MST 2010
Hello,

I downloaded and installed the LPCExpresso tools and all went well, but when I try to debug designs larger than 8k, I get a message that the design is too large for the license .. ?

i checked that the license is correctly installed and get the message that it is and I should be able to work with designs up to 128k.

I tried to uninstall, restart and reinstall the tools, but no luck.

I use WinXP SP3 Danish version on IBM ThinkPad T41p

Best regards
0 件の賞賛
返信
3 返答(返信)

1,137件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Wed Dec 29 09:09:33 MST 2010
In the first place, try fixing the write access:

http://support.microsoft.com/kb/308419
0 件の賞賛
返信

1,137件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jespern on Wed Dec 29 08:33:09 MST 2010
Hello,

You are right - the directory is write protected - but it seems that I cannot remove the protection, and the references do not mention how it is done.

The file cscript.exe is in \Windows\System32 but I don't know how to check if it is blocked and the references are pretty vague about how to check and fix this.

So, please, can you help here ?

regards



Quote: CodeRedSupport
This can be due to:
1. Write protection enabled for the "/Documents and Settings/All Users/LPCXpresso" directory.
2. cscript execution is disabled, inhibited by a virus checker, or cscript.exe is not in your system path.Typically, this executable is located in the "\Windows\System32" directory.

Please review these threads for additional information:

http://knowledgebase.nxp.com/showthread.php?t=855
http://knowledgebase.nxp.com/showthread.php?t=169

0 件の賞賛
返信

1,137件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Mon Dec 27 10:54:01 MST 2010
This can be due to:
1. Write protection enabled for the "/Documents and Settings/All Users/LPCXpresso" directory.
2. cscript execution is disabled, inhibited by a virus checker, or cscript.exe is not in your system path.Typically, this executable is located in the "\Windows\System32" directory.

Please review these threads for additional information:

http://knowledgebase.nxp.com/showthread.php?t=855
http://knowledgebase.nxp.com/showthread.php?t=169





Quote: jespern
Hello,

I downloaded and installed the LPCExpresso tools and all went well, but when I try to debug designs larger than 8k, I get a message that the design is too large for the license .. ?

i checked that the license is correctly installed and get the message that it is and I should be able to work with designs up to 128k.

I tried to uninstall, restart and reinstall the tools, but no luck.

I use WinXP SP3 Danish version on IBM ThinkPad T41p

Best regards

0 件の賞賛
返信