LPCexpresso MB1700 example not build properly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCexpresso MB1700 example not build properly

2,920 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by terrype on Mon Sep 01 03:53:52 MST 2014
Dear Members, I downloaded "mcb1700.code_.bundle.lpc1769.lpcxpresso",  I  import the project inside the LPCexpresso and build all project.
All the project having build error

cannot find -lCMSISv2_LPC17xx
collect2.exe: error: ld returned 1 exit status

looks like board related software missing, is any one facing a similar problem
0 Kudos
Reply
8 Replies

2,890 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by terrype on Tue Sep 02 16:15:59 MST 2014
Hi LabRat,  Yes i did.
Thanks Lab suppor. I can build the board support package, but don't you thnk that LPC Open team can spend time and provide the package for wider audinace. Also it is good time to provide C++ project in LPC Open
LPCOpen is one of the best support providers for application developers to getting started without spending lot of time to understand the chipset and board detail and expecting you to continue the great work.
Thanks in advance




regards
terry
0 Kudos
Reply

2,890 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Sep 02 00:56:05 MST 2014
The MCB1700 examples were developed BEFORE LPCOpen and use CMSIS instead. Therefore, these examples do not have board and chip files.

For starting a new development, I would recommend using LPCOpen. Unfrtunatley, there is not a port of LPCOpen for the MCB1700 board, but it is relatively easier to do, starting from the board files for another board.
0 Kudos
Reply

2,890 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon Sep 01 17:06:51 MST 2014

Quote: terrype
The MB1700 LPC exresso bundle does not have chip and board related project.  I am not sure whether i am making a any mistake here...



This sample is an old  CMSIS2.0 sample, not a LPCOpen sample. This old samples don't use board files...
0 Kudos
Reply

2,890 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon Sep 01 16:58:22 MST 2014
Did you build CMSIS library before you are using it in your project?

See: http://www.lpcware.com/content/faq/lpcxpresso/linker-cannot-find-library
0 Kudos
Reply

2,890 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by terrype on Mon Sep 01 16:51:26 MST 2014
Good morning, Thanks for the response.  The link you send me is working well but that link for the LPCexpresso board (LPC1769 board from Embedded Aritisis).
I am talking aout

the board from keil
http://www.keil.com/mcb1700/

the project from LPC Open

http://www.lpcware.com/content/nxpfile/mcb1700-sample-code-bundle-lpc1769-peripherals-using-lpcxpres...

In LPCOpen (Lpcware) released the project(.zip) file they include
1. Cortex M3
2. LPC17xx chip
3. LPC17xx board
then application,  Is it correct?
The MB1700 LPC exresso bundle does not have chip and board related project.  I am not sure whether i am making a any mistake here , please test and let me know




0 Kudos
Reply

2,890 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Sep 01 06:02:40 MST 2014
I just checked that download. The CMSIS library *IS* supplied in the download. Perhaps you didn't build it correctly. See
http://www.lpcware.com/content/faq/lpcxpresso/linker-cannot-find-library
0 Kudos
Reply

2,890 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by terrype on Mon Sep 01 05:22:26 MST 2014
Thanks for the response,  LPCware zip file suppose to contain all the necessary files and library, is it correct?
Why can you put all necessary files into the zip file?

I think apps team did not know the problem,  as a support team, please inform to apps team and they will fixed this problem
0 Kudos
Reply

2,890 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Sep 01 04:41:46 MST 2014
You will need to add the correct CMSIS library to your workspace.

See:
http://www.lpcware.com/content/faq/lpcxpresso/cmsis-support
0 Kudos
Reply