LPCXpresso1769 Examples

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso1769 Examples

1,197 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SebastianKulik on Wed Apr 27 09:44:15 MST 2011
Hi,

I cant find examples especially for LPCXpresso1769 as standalone (not MCB1700 and so on).
Something like easy "Blinky" for onboard LEDs, means onboard hardware.
Can someone help?
Thx a lot!
0 项奖励
回复
4 回复数

1,181 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Wed Apr 27 11:47:52 MST 2011
Changing project MCU target:

http://support.code-red-tech.com/CodeRedWiki/ChangingProjectTarget
0 项奖励
回复

1,181 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Wed Apr 27 11:38:23 MST 2011
AFAIK, and LPC1769 is the same as an LPC1768 except it has a higher maximum clock speed (120Mhz vs 100Mhz).
0 项奖励
回复

1,181 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SebastianKulik on Wed Apr 27 10:11:03 MST 2011

Quote: Zero
What's wrong with LPCXpresso1768_systick sample in LPCXpresso1768.zip (--> Example folder) ?


Yes, it works too, actually all 1768 projects seems to work.
Maybe it exists some new things for 1769?

Another question: Ive registered IDE and see "Full license, 128k", but try to use Program Flash see error somting like: your license not allowed Flash command line (or something like that) -any idea?

THX
0 项奖励
回复

1,181 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Wed Apr 27 09:54:57 MST 2011
What's wrong with LPCXpresso1768_systick sample in LPCXpresso1768.zip (--> Example folder) ?
0 项奖励
回复