LPCXpresso with LPC-Link2 jtag

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso with LPC-Link2 jtag

6,523 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aferrari on Wed Aug 05 05:19:56 MST 2015
Hello everybody,

I'm using LPCXpresso (v7.0.2 on windows XP) with "LPC4088 QuickStart Board".

In order to download and debug the firmware, I'm trying to use the "LPC-Link 2" debug adapter.

I'm using the J8 connector on the "LPC-Link 2" connected to the J7 connector on the "LPC4088 QuickStart Board".

When I try do debug the project, LPCXpresso doesn't recognize the "LPC-Link 2" debugger (see attached picture).

The hardware manager shows that the "LPC-Link 2" is correctly installed.

Do you have any idea in order to fix this issue?

Many thanks in advance

Alberto
0 项奖励
回复
8 回复数

6,384 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aferrari on Thu Aug 06 07:03:00 MST 2015
Dear Support,

thanks again for your help.

In the FAQ I've found the solution.

The problem was a too long USB cable between the PC and the LPC-Link2 board.

The cable is good because I normally use it with another debugger, but when I changed it with a shorter one everything started working fine.

Thanks a lot.

Have a nice day

Alberto
0 项奖励
回复

6,384 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Aug 06 02:03:17 MST 2015
Read this FAQ:
https://www.lpcware.com/content/faq/lpcxpresso/booting-lpc-link2

Especially the Troubleshooting guide at the end.
0 项奖励
回复

6,384 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aferrari on Thu Aug 06 01:39:45 MST 2015
Dear Support, thanks for the hints.

I've moved to Windows8 with the latest LPCXpresso version 7.9.0 (see attached picture LPCXpresso_1.JPG).

I'm always using lpc4088-quickstart-board with LPC-Link 2.

When I try to download and debug the software (by means "Debug 'test1' button), the "LPC based USB device" disappears from the device manager and LPCXpresso stops at 95% (see attached picture LPCXpresso_2.JPG).

Do you have any idea about this issue?
0 项奖励
回复

6,384 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Aug 05 08:49:44 MST 2015
You need to soft-boot LPC-Link2 with the Redlink image. This is done automatically by LPCXpresso 7.0.2 when
- JP1 is removed
- you power-cycle LPC-Link2 after removing JP1

JP2 is supplying target power and should NOT be inserted if the target is already being supplied with power.

LPCXpresso will automatically detect the Debug Adapter. If the project has been configured to use CMSIS-DAP, you can just "Search for any enabled emulator" when prompted the configuration will be reset.

As 7.0.2 is obsolete, and we do not have Windows XP here, we will be unable to provide any further assistance on this topic.
0 项奖励
回复

6,384 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aferrari on Wed Aug 05 07:28:40 MST 2015
Don't worry, but I've already tried different combination of JP1 and JP2.

Could you tell me the right combination of JP1 and JP2 on LPC-Link2 and JP3 on LPC4088 (for example JP1 removed, JP2 inserted and JP3 removed)?

About the LPCXpresso there is some setting to do?
For example I've seen that is possible to select the emulator and the debug template (see attached picture)
0 项奖励
回复

6,384 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Aug 05 07:08:59 MST 2015
Sorry, that should have been JP1. See
https://www.lpcware.com/content/faq/lpcxpresso/lpc-link2-support

0 项奖励
回复

6,384 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by aferrari on Wed Aug 05 06:58:31 MST 2015
Hi Support,

thanks for the hint.

I'd like to use LPCXpresso 7.0.2 because of I'm using windows XP.

I've tried with JP2 removed on LPC-Link2 (see attached picture), but the result is the same.

Any other suggestion?

Alberto
0 项奖励
回复

6,384 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Aug 05 05:49:16 MST 2015
LPCXpresso 7.0.2 does not support CMSIS-DAP. If you must use that version of LPCXpresso, you must let it soft-boot LPC-Link2 by removing J2.
0 项奖励
回复