LPCXpresso programmer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso programmer

1,442件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Charles on Thu Mar 25 14:11:34 MST 2010
Does code_red have an application to program LPC devices using the LPC-Link debug interface so we don't have to load the IDE?

I would like to program our device with code sent to us from a contractor so we can test the firmware while the contractor continues with the development.
0 件の賞賛
返信
4 返答(返信)

1,346件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bladerunner on Mon Mar 29 04:25:38 MST 2010

Quote: Charles
Does code_red have an application to program LPC devices using the LPC-Link debug interface so we don't have to load the IDE?

I would like to program our device with code sent to us from a contractor so we can test the firmware while the contractor continues with the development.



You could also use Flashmagic to program it.
0 件の賞賛
返信

1,346件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Fri Mar 26 01:00:25 MST 2010
It is currently in beta, so hopefully, RSN.
0 件の賞賛
返信

1,346件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Charles on Fri Mar 26 00:36:04 MST 2010
Thanks,

When do you expect the next release?
0 件の賞賛
返信

1,346件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Mar 25 14:13:25 MST 2010
This feature will be coming in the next release.
0 件の賞賛
返信