LPCXpresso is not getting Registerd

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso is not getting Registerd

709 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP86278 on Sun Sep 07 21:56:13 MST 2014
Dear All,

I register LPCXpresso free addition and it is showing the full version now. But when I am trying to flash code into the controller it is showing licence error although file size is less than 100kB. I faced this issue with all the version. What I have to do with get the free full version
0 项奖励
回复
1 回复

703 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun Sep 07 23:43:16 MST 2014
In the first place, please see:

http://www.lpcware.com/content/faq/lpcxpresso/flash-image-too-large

Regards,
LPCXpresso Support
0 项奖励
回复