LPCXpresso is not getting Registerd

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso is not getting Registerd

707件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP86278 on Sun Sep 07 21:56:13 MST 2014
Dear All,

I register LPCXpresso free addition and it is showing the full version now. But when I am trying to flash code into the controller it is showing licence error although file size is less than 100kB. I faced this issue with all the version. What I have to do with get the free full version
0 件の賞賛
返信
1 返信

701件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun Sep 07 23:43:16 MST 2014
In the first place, please see:

http://www.lpcware.com/content/faq/lpcxpresso/flash-image-too-large

Regards,
LPCXpresso Support
0 件の賞賛
返信