LPCXpresso debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso debug

1,198件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sharadanand on Wed Nov 30 01:31:02 MST 2011
I want to debug my code without connecting development board
but when I try to debug locally IDE gives error, what could be the reason?
0 件の賞賛
返信
4 返答(返信)

1,191件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sharadanand on Wed Nov 30 03:10:40 MST 2011
OK
thanks for the help:)
0 件の賞賛
返信

1,191件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Wed Nov 30 03:08:45 MST 2011
It is not 'a kind of simulation' it IS simulation!

LPCXpresso requires real hardware.
0 件の賞賛
返信

1,191件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sharadanand on Wed Nov 30 03:03:08 MST 2011
I thought it should work like KEIL where you can test the code without any hardware. It is a kind of simulation
0 件の賞賛
返信

1,191件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Wed Nov 30 02:43:11 MST 2011
What are you expecting to happen if you have no board to debug? There is no simulator in LPCXpresso - it works with real hardware.
0 件の賞賛
返信