LPCXpresso and GCC?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso and GCC?

713 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Mark_O on Fri Feb 12 19:40:46 MST 2010
I've looked in both the KnowledgeBase and done a search of the Forum, but was unable to find the answer to a question I had.  Regarding this, from the main page on LPCXpresso:

"[I]LPCXpresso is based on Eclipse with many LPC-specific enhancements. It also features the latest version of the industry standard GNU tool chain with a proprietary optimized C library...[/I]"

Is C the only language from the GNU Compiler Collection that is supported?  Or are the rest as well?  I.e., C++, Objective-C, and plug-in front-ends like Pascal?

Thanks,

- Mark
0 项奖励
回复
1 回复

661 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Feb 13 03:11:41 MST 2010
Only C is supported directly in the IDE, although the C++ compiler is also provided. No other languages are supported.
0 项奖励
回复