LPCXpresso and Complex Numbers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso and Complex Numbers

697 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Orac on Sun Jun 14 09:04:55 MST 2015
Hi All,

I'm writing a grid tied application for the LPC4370 and wish to use Complex Numbers in my PLL routine.

I try and include <complex.h> but the compiler can't find it.

I've found several in the tool chain file structure including:

lpcxpresso_7.4.0_229/lpcxpresso/tools/arm-none-eabi/include/

I presume the Redlib library which is being used doesn't contain it, but I have also tried the others without any success.

Can anyone point me in the right direction please?

Regards and many thanks
Pete
0 Kudos
Reply
1 Reply

635 Views
lpcware
NXP Employee
NXP Employee
0 Kudos
Reply