LPCXpresso Preferences Location

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso Preferences Location

943件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Sat Aug 16 13:04:49 MST 2014
I have installed IDE 7.3 to a new directory; 6.2 is still installed in a separate directory as a fallback.

Apart from asking for a workspace, 7.3 seems to have inherited all my window placement, colours, fonts etc.
Including the activation details.
This is GOOD, but I had understood that parallel installations of the IDE were totally separate.

Where are these preferences saved, as I am about to update my Windows OS on a new hard disk;
I don't want to have to set all the preferences again as some of them are buried quite deeply in menus and are
not always in expected places. And I can't actually remember exactly what preferences I altered.

So, to be specific, what file or files hold the preferences, and what directory(ies) store the files.

Regards, Mike.
0 件の賞賛
返信
3 返答(返信)

922件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon Aug 18 04:00:03 MST 2014
Not sure what required file/directories you are talking about. As FallGuy says, just use the Export/Import functionality to transfer preferences from one workspace to another.

Else, try using your favourite search engine for something like "eclipse transfer preferences to another workspace"

Regards,
LPCXpresso Support.
0 件の賞賛
返信

922件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Sun Aug 17 15:41:14 MST 2014
Thanks FallGuy, it would be nice to have a list of required files and directories though; maybe NXP will chip in.
0 件の賞賛
返信

922件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TheFallGuy on Sun Aug 17 10:22:56 MST 2014
That are stored in the workspace.

You can export the preferences. See
http://help.eclipse.org/indigo/index.jsp?topic=%2Forg.eclipse.wb.doc.user%2Fhtml%2Fpreferences%2Fpre...
0 件の賞賛
返信