LPCXpresso Licensing Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso Licensing Issue

861件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by hackster84 on Sun Apr 14 16:20:52 MST 2013
Hi,

I'm having a licensing issue.  I have LPCXpresso installed correctly on my machine with the license fully activated and I'm getting an error when I try to upload projects larger than 8 k to my LPCXpresso 1114 board.  The error reads as follows:

"License restriction: Flash image too large for this license. "

The image is only about 9k... when I try to upload a small file (under 8 k) the console reads that I'm using an unregistered license and that I have an upload limit of 8k.  Now, when I use the help menu to look at my license status, this is what it reads:

"License type: FULL
Debug limit: 128k
Activation code: xxxxxxxxx

A FULL copy of LPCXpresso may be used for production."

Anybody have any ideas on how to fix this issue?  Thanks in advance for your help.

-Chris
0 件の賞賛
返信
1 返信

851件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Sun Apr 14 23:36:03 MST 2013
Read the sticky post on top of the forum and do a search. This topic has been answered before.
Have you read the FAQ on the Code-Red website?
0 件の賞賛
返信