LPCXpresso LPC11C24 Rev B - USB Driver Problem with Win 7 (64Bit)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso LPC11C24 Rev B - USB Driver Problem with Win 7 (64Bit)

738件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by user456793 on Tue Jan 12 09:28:15 MST 2016
Hi,

my LPCBoard, LPCXpresso LPC11C24 Rev B, is not booting with the LPC-Link Firmware on my Windows 7 (64 Bit) PC.
I can see the USB Device with DFU Capabilities, when I connect the board.
But when I try to programm it with "bootLPCXpresso.cmd hid" from the script directory, I get the message "Device does not support DFU" or the dfuapp.exe doesn't come to an end, so that I have to kill the dfuapp.exe.
I tried: different USB cable, with and without USB Hub, software version LPCXpresso_6.1.0_164 and LPCXpresso_8.0.0_526, and even a second LPCXpresso board.
What else can I do?

Thanks

Steffen
0 件の賞賛
返信
1 返信

700件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Tue Jan 12 09:49:00 MST 2016
Read this FAQ?
https://www.lpcware.com/content/faq/lpcxpresso/booting-lpc-link
0 件の賞賛
返信