LPCXpresso Installation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso Installation

1,071 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DeniseJ on Tue Aug 12 08:03:29 MST 2014
Can anyone help with this error installing v7.3.0 on Windows 7 x64.  LPCXpresso starts to launch, displays splash screen, prompt for workspace, then nothing afterwards.  Following error is in event\application log, machine has redist 2005,2008,2010 and 2013, 2013 was installed during LPCXpresso installation:

Log Name:      Application
Source:        Application Error
Date:          12/08/2014 15:03:57
Event ID:      1000
Task Category: (100)
Level:         Error
Keywords:      Classic
User:          N/A
Computer:      MI999-A05.unv.wlv.ac.uk
Description:
Faulting application name: lpcxpresso.exe, version: 0.0.0.0, time stamp: 0x50816486
Faulting module name: MSVCR100.dll, version: 10.0.40219.1, time stamp: 0x4d5f0c22
Exception code: 0xc0000409
Fault offset: 0x0001ec6b
Faulting process id: 0xef0
Faulting application start time: 0x01cfb6363dbdb3fd
Faulting application path: C:\nxp\LPCXpresso_7.2.0_153\lpcxpresso\lpcxpresso.exe
Faulting module path: C:\windows\system32\MSVCR100.dll
Report Id: 803f8ffd-2229-11e4-bd5b-7071bc42ad8e
0 Kudos
Reply
2 Replies

1,038 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by DeniseJ on Wed Aug 13 03:55:12 MST 2014
Version installed yesterday was 7.2.0, tried installing the C++2010 redist but still had same issue.  Tested latest 7.3.0 today which has worked without issues the dll error. 
0 Kudos
Reply

1,038 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Aug 12 08:17:06 MST 2014
Can you try downloading and installing the latest x86 version of the MSVC redistributable from here:
http://www.microsoft.com/en-us/download/details.aspx?id=8328

Yes, I do mean the x86 and NOT the x64 version.

Please let us know if this solves your problem.
0 Kudos
Reply