LPCXpresso IDE Function Preview Colors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso IDE Function Preview Colors

1,583件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by steven_ece on Thu May 10 10:04:41 MST 2012
Hello,

When I hover over a function call I can see the function implementation preview, but the colors inhibit me from seeing all the code. How do I change the colors used in the preview window? Thanks!
0 件の賞賛
返信
4 返答(返信)

1,563件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by steven_ece on Fri May 11 09:30:30 MST 2012
Thank you! That did the trick. :)
0 件の賞賛
返信

1,563件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu May 10 13:13:05 MST 2012
Which OS are you running? If Linux, then you might want to see:

http://support.code-red-tech.com/CodeRedWiki/Linux_GUI_Issues

Regards,
CodeRedSupport
0 件の賞賛
返信

1,563件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by steven_ece on Thu May 10 12:59:45 MST 2012
Thanks!

I looked here and could not deduce which color setting I needed to change. I ended up downloading a theme @ eclipsecolorthemes that allowed me to see the code. I still would like to be able to view these function previews with the default theme.
0 件の賞賛
返信

1,563件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by frame on Thu May 10 11:38:35 MST 2012
This is Eclipse, and Eclipse is a PITA in this regard (my opinion...).

Look in the menu [B]Window->Preferences[/B], and change there in the items '[B]General[/B]' and [B]'C/C++[/B]' all '[B]Editor[/B]' - options to your preferences.

This is always one of the first thing I do. I hate it if an IDE/editor assumes it knows better than me what I want.
0 件の賞賛
返信