LPCXpresso Free Edition limits

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso Free Edition limits

910 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lukos on Mon Mar 31 13:51:16 MST 2014
Hello

The LPCXpresso Free Edition supports the [u]download[/u] limit up to 256k.
Does it mean LPCXpresso is able to [u]generate[/u] the bigger code than 256k but without possibility to download it to target?

Is the statement "A FULL copy of LPCXpresso (Free Edition) may be used for production." means the software can be used in commercial application?

Thanks
Luk
0 Kudos
Reply
1 Reply

821 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon Mar 31 14:03:01 MST 2014

Quote: lukos
Does it mean LPCXpresso is able to [u]generate[/u] the bigger code than 256k but without possibility to download it to target?



Yes.

Quote: lukos
Is the statement "A FULL copy of LPCXpresso (Free Edition) may be used for production." means the software can be used in commercial application?



Of course.
0 Kudos
Reply