LPCXpresso Free Edition limits

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso Free Edition limits

911 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lukos on Mon Mar 31 13:51:16 MST 2014
Hello

The LPCXpresso Free Edition supports the [u]download[/u] limit up to 256k.
Does it mean LPCXpresso is able to [u]generate[/u] the bigger code than 256k but without possibility to download it to target?

Is the statement "A FULL copy of LPCXpresso (Free Edition) may be used for production." means the software can be used in commercial application?

Thanks
Luk
0 项奖励
回复
1 回复

822 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon Mar 31 14:03:01 MST 2014

Quote: lukos
Does it mean LPCXpresso is able to [u]generate[/u] the bigger code than 256k but without possibility to download it to target?



Yes.

Quote: lukos
Is the statement "A FULL copy of LPCXpresso (Free Edition) may be used for production." means the software can be used in commercial application?



Of course.
0 项奖励
回复