LPCXpresso Free Edition limits

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso Free Edition limits

909件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lukos on Mon Mar 31 13:51:16 MST 2014
Hello

The LPCXpresso Free Edition supports the [u]download[/u] limit up to 256k.
Does it mean LPCXpresso is able to [u]generate[/u] the bigger code than 256k but without possibility to download it to target?

Is the statement "A FULL copy of LPCXpresso (Free Edition) may be used for production." means the software can be used in commercial application?

Thanks
Luk
0 件の賞賛
返信
1 返信

820件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon Mar 31 14:03:01 MST 2014

Quote: lukos
Does it mean LPCXpresso is able to [u]generate[/u] the bigger code than 256k but without possibility to download it to target?



Yes.

Quote: lukos
Is the statement "A FULL copy of LPCXpresso (Free Edition) may be used for production." means the software can be used in commercial application?



Of course.
0 件の賞賛
返信