LPCXpresso Flash programming display log - explain

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso Flash programming display log - explain

748件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sgg06786 on Thu May 07 17:53:30 MST 2015
Hi

Can you please help to explain the below last few lines of execution log? I would like to know what happen after the successful "Flash write Done".


Nt: Erased/Wrote page  0-6 with 25052 bytes in 4047msec
Pb: (100) Finished writing Flash successfully.
Nt: Flash write Done
Xe:
Ed:06: File 'BPMA_CGW_Appl_V00.11.bin' load failure: Ee(07). Bad ACK returned from status - wire error.
Wc: SWD Frequency (Final): 50 KHz.
Pc: (100) Target Connection Failed


Thank you.
0 件の賞賛
返信
1 返信

731件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri May 08 00:23:00 MST 2015
Sorry, but you haven't given us sufficient information.

Which target chip? Which debug probe? Which version of LPCXpresso? Are you debugging or running the Flash dialog?

Have you tried this?
http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access
0 件の賞賛
返信