LPCXpresso Cortex M0 - Embedded Web Server

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso Cortex M0 - Embedded Web Server

1,607 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kmmankad on Thu Mar 24 07:21:31 MST 2011
Hi,
as part of the recent campaign, "Breaking the 8/16 bit habit",I am going to get my own LPC Xpresso Cortex M0 board..
I saw this entry to the LPC 1100 design challenge,"Remote Home Automation controller",which has mention of a similar embedded webserver design.
Unfortunately,I havent been able to reach the author,and the project is poorly documented.

Could someone guide me to code examples on the ethernet side with the free LPC Xpresso Cortex M0 board?
0 Kudos
Reply
5 Replies

1,513 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Fri Mar 25 10:45:37 MST 2011
This project doesn't use internal Ethernet block (like LPC176x) because it has no internal Ethernet block. So it must use some kind of external Ethernet block.
0 Kudos
Reply

1,513 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kmmankad on Fri Mar 25 10:30:56 MST 2011

Quote: larryvc
UM10398
Chapter 10: LPC111x/LPC11Cxx UART
Rev. 4 — 4 March 2011 User manual

True no ethernet block but external works.




Didnt get you.. "external works" ??
0 Kudos
Reply

1,513 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Thu Mar 24 09:38:05 MST 2011

Quote: Luis Digital

LPC111x not have ethernet.



UM10398
Chapter 10: LPC111x/LPC11Cxx UART
Rev. 4 — 4 March 2011 User manual

True no ethernet block but external works.
0 Kudos
Reply

1,513 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Thu Mar 24 08:38:53 MST 2011
http://www.lpc1100challenge.com/viewentries/list?order=desc&field=total_rating&category_status=4
0 Kudos
Reply

1,513 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Thu Mar 24 08:18:46 MST 2011
Hello,

LPC111x not have ethernet. Do you have a link to the project?

I ordered several LPC1764, with ethernet, to create low-cost boards.

I'm just waiting for approval. I filled out a form on which I agree not to develop weapons of mass destruction. lol
0 Kudos
Reply