LPCXpresso, Code Red web site ping

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso, Code Red web site ping

1,946件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Sat Feb 11 13:40:25 MST 2012
Unfortunately, but I have to block the IP [FONT=Arial]67.222.22.2[/FONT] (Code Red web site), because LPCXpresso pings each time it starts.

Any option to disable it?
0 件の賞賛
返信
7 返答(返信)

1,907件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Mon Feb 13 12:06:39 MST 2012
I have two conclusions, based on your comments:
1- If "A" spy me, everybody can spy on me and everything is correct.
2- Code Red IDE needs Internet to function (I do not think that is the case because I have more than 24 hours using it with the lock.).
0 件の賞賛
返信

1,907件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Mon Feb 13 11:44:30 MST 2012
Pong went back to the future, all the way back to 1972 to meet Allan Alcorn :D

If you would not like to be spied upon, the best thing I can recommend is to disconnect your computer from the network, run it solely on your own power source (someone could identify what you are doing by reading a power surge profile) and hide in a location that absolutely does not allow any signals to be transmitted to someone spying you with an RF sniffer :eek:

Actually it is not that hard to see what the LPCXpresso tools send to code-rec-tech.com at all. I'd be happy to show you, but then I would also show you my IP number and some more information about my system :p and I don't like that.
I think it's OK to send the information to code-red-tech.com (it is actually just checking the license) but you are right when you do not want to share too much information about your computer (or your IP location) on the internet.

You are using the internet, you are even using the LPCXpresso forum. Lot's of website (knowledgebase.nxp.com is no exception on this rule) communicate cookies with your PC. These cookies contain information about your username, the time since your last visit, maybe even other information like the last visited page at the site and much more.
I am sometimes scared about all these cookies (most cookies are delicacies for the websites I am visiting but not for me).

I would not bother too much about this 'ping' in LPCXpresso. If you block this, don't blame Code Red or us when things suddenly stop working...

Regards,

Rob

P.s: do you have any idea what kind of information Google, Ebay and PayPal are collecting about you. Just look at their policies and then get scared :eek:
0 件の賞賛
返信

1,907件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Mon Feb 13 07:02:15 MST 2012

Quote: Polux rsv
Anything different than any other software which check for updates each time it is lunched ?

Angelo



Should I be using another program, because mine never informed me of updates.

Even being so, the programs have options to disable these functions.
0 件の賞賛
返信

1,907件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Polux rsv on Mon Feb 13 05:12:46 MST 2012
Being a "hardware guy", I probably missed some points.
What's different on Code Red  IDE ?
Anything different than any other software which check for updates each time it is lunched ? Anything which could not be blocked by the firewall or anti-virus ???

Angelo
0 件の賞賛
返信

1,907件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Sun Feb 12 14:26:55 MST 2012

Quote: Polux rsv
What's wrong with that "ping" ?

Angelo



Actually the port used is 80 (WWW), so I guess it's not a simple "ping".

I have not reviewed the contents of the package, but the IP I have it blocked in my router.

Otherwise, if you would like to be spied no problem.:)
0 件の賞賛
返信

1,907件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Feb 12 12:53:45 MST 2012
And where's the 'pong' :rolleyes:
0 件の賞賛
返信

1,907件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Polux rsv on Sun Feb 12 12:43:44 MST 2012
What's wrong with that "ping" ?

Angelo
0 件の賞賛
返信