LPCXpresso Board With CAN Controller?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXpresso Board With CAN Controller?

1,217件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rtos on Sat Feb 13 16:38:31 MST 2010
Is there an LPCXpresso board that has a [B]CAN Controller[/B]? Something with the LPC1764 or similar?

If not, is there a drop-in compatible LPC with a CAN Controller that I could swap onto the LPCXpresso LPC 1343 board?

Thanks.
0 件の賞賛
返信
4 返答(返信)

1,207件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by annodomini2 on Mon Feb 15 16:08:27 MST 2010
Yup, mbed has a cloud based online IDE and compiler with a reasonable library set.

Or you can use Eclipse and YAGARTO or one of the other ARM compiler toolchains.

Yes the JTAG cannot be used with an mbed the JTAG interface is used by its programming interface.
0 件の賞賛
返信

1,207件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rtos on Sun Feb 14 06:53:44 MST 2010
I think I found the answer in another post:


Quote:

The mbed board does not have debugger connections on it, so it cannot be  connected to an external debugger such as the LPCXpresso LPC-LINK.  However the LPCXpresso IDE can generate binary files which can be  programmed into the mbed board over the USB connection.
Quote:

0 件の賞賛
返信

1,207件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rtos on Sun Feb 14 06:25:49 MST 2010

Quote: annodomini2

There's the MBED if you want CAN.



Thanks.  Can the MBED be used with the LPCXpresso programmer and compiler?  Or is it locked into using their online compiler?
0 件の賞賛
返信

1,207件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by annodomini2 on Sun Feb 14 03:35:27 MST 2010
Not at this time, NXP are doing some LPC11 series with CAN later this year.

There's the MBED if you want CAN.

Or a number of other LPC17xx series dev boards with CAN.

Unless an ARM7 is acceptable then there's devices such as the LPC2109. LPC2129

Other manufacturers include STM32F103

Or conversely you can add an SPI CAN controller to the LPC11 or LPC13
0 件の賞賛
返信