LPCXpresso 8.1.4 doesn't show opcode in disassembly view when debugging

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso 8.1.4 doesn't show opcode in disassembly view when debugging

729 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by dariy on Mon Apr 18 13:20:12 MST 2016
Everything works fine. Just the opcode wouldn't show up in debug mode following [u]Disassembly View and instruction level debugging[/u]
The Memory View and the disassembly file look fine.

Show Opcodes on the right-click context menu (in the address column) will add/remove a few pixels between the address and the rest of the line, but does not show the opcode bytes.
0 项奖励
回复
3 回复数

687 次查看
lpcware
NXP Employee
NXP Employee
bump
0 项奖励
回复

687 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Thu Apr 21 21:57:05 MST 2016
Glad that this issue is finally getting some attention, I reported it as far back as version 6 and version 7.
Cheers, Mike.
0 项奖励
回复

687 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Apr 19 07:10:11 MST 2016
Hi Dt,

Thanks for bring this to our attention.  We have replicated the issue here and it is under investigations for fixing in a future release.

Ciao,
LPCXpresso Support.
0 项奖励
回复