LPCXPRESSO base board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCXPRESSO base board

1,169件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Sharadanand on Sat Nov 26 00:40:25 MST 2011
Is LPCXPRESSO base board is compatible with all LPCXPRESSO board?
0 件の賞賛
返信
3 返答(返信)

1,154件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Sun Nov 27 08:34:17 MST 2011
I've created a nice little overview of the pinout for the different LPCXpresso modules.
See this page for the pinning of the different modules.
I've compared all other modules against the LPCXpresso 1343 since that module's names are being used on the base board.
[INDENT]Rob
[/INDENT]P.s: how do we get rid of the "thumbs down" with this thread?
0 件の賞賛
返信

1,154件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Sun Nov 27 05:29:39 MST 2011
Yup,

I think that was the whole idea of LPCXpresso: a common platform with different controller boards.

Of course not all board have the same functionality so you will discover that the RJ45 ethernet connection has no use with an lpc1343 board.

It does help to look at the schematics of both the base board and the LPCXpresso modules. On the lpc1769 the I/O pins are placed different from the lpc1114 and 1343 modules.
The labels next to the expansion connector on the LPCXpresso base board are for lpc1114/1343 units: P2.11 on the base board (SCK on the lpc1343) is actually P0.7 (SCK1) on the lpc1769

My lpc1769 module is due to arrive next week - guess it's time to make a nice overview :rolleyes:

Rob
0 件の賞賛
返信

1,155件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sat Nov 26 03:13:24 MST 2011

Quote:

This Base Board can be bought in a kit together with a LPCXpresso LPC1xxx board for a discounted price.
    LPC1114 LPCXpresso Board
    LPC11C24 LPCXpresso Board
    LPC11U14 LPCXpresso Board
    LPC1227 LPCXpresso Board
    LPC1343 LPCXpresso Board
    LPC1769 LPCXpresso Board
    mbed Board

See: http://www.embeddedartists.com/products/lpcxpresso/xpr_base.php

So the answer is: YES :eek:
0 件の賞賛
返信