LPCScrypt latest release : 1.7.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCScrypt latest release : 1.7.0

1,152 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Feb 23 02:35:06 MST 2016
LPCScrypt is a command-line based, fast flash, EEPROM, OTP and security programming tool for the LPC1800 and LPC4300 series of microcontrollers.

It now also provides functionality to program LPC-Link2 and LPCXpresso V2/V3 debug probe firmware (replacing the LCT - Link2 Configuration Tool).

For more details, please visit: http://www.lpcware.com/LPCScrypt

[h2]Latest release : v1.7.0 build 696, 23 Feb 2016[/h2]

[list]
[*]Added flashSet command (as a superset and replacement of EEPROMset) to enable patching of word in all supported flash memories
[list]
[*]usage -  flashSet flash+offset value
[/list]
[*]CMSIS-DAP programming script displays probe serial number/ID
[*]Updated binary for CMSIS-DAP debug probe firmware incorporating new features (to ..V5_147):
[list]
[*]support for power measurement averaging with specific LPCXpresso V3 boards
[*]probes enumerate as unique devices by adding an ascii representation of the debug probe MCU's serial number
[/list]
[*]Various minor bug fixes
[/list]

[h2]Previous releases[/h2]

[h3]v1.6.0 build 652, 26 Nov 2015[/h3]

[list]
[*]Added automatic verify of all flash programming operations.
[*]Added commands for various SPIFI operations.
[*]Updated binary for CMSIS-DAP debug probe firmware with new features (to ..V5_134)
[list]
[*]Including support for ISP Reset over debug
[/list]
[*]Updated binary for Segger J-Link debug probe firmware (to ..V20151006)
[*]Added support for new SPIFI device – Micron N25Q128
[*]Various minor bug fixes, including:
[list]
[*]Correctly programs memories where size is not a power of 2.
[*]PartID word 2 now fully displayed.
[/list]
[/list]

[h3] v1.5.2 build 588, 23 June 2015[/h3]

[list]
[*]Windows only: added Start menu shortcuts for scripts to boot LPCScrypt and to program debug probe firmware.
[*]Windows only: added CMSIS-DAP drivers to drivers directory.
[*]Improved scripts to program debug probe firmware.
[*]Various minor bug fixes, including:
[list]
[*]host app now correctly handles [memory_name + offset] calculation
[*]SPIFI size corrected for W25Q128FV
[/list]
[/list]

[h3] v1.5.0 build 562, 1 June 2015[/h3]

[list]
  [*]Added binaries for CMSIS-DAP and Segger J-Link debug probe firmware
[list]
  [*]Note: the CMSIS-DAP version supplied (v5.112) supersedes the version supplied with LCT (v2.02).
[/list]
  [*]Added scripts to enable easy programming of CMSIS-DAP and J-Link firmware
  [*]Added Debug Probe Firmware Programming guide
  [*]Added support for new SPIFI devices – W25Q128FV and MX25L1606
[/list]

[h3] v1.3 build 496, Mar 12 2015[/h3]

[list]
  [*]Added support for connections via USB1 as well as USB0.
  [*]Added support for new SPIFI devices – W25Q40CV and PM25LQ032C.
  [*]Fixed issue with download of binaries which are not a multiple of 4 bytes in size.
  [*]Improved error handling when host could not gain control of target device.
  [*]Updated documentation to reflect maximum image size for secure boot.
[/list]

[h3] v1.2 build 435, Jan 29 2015 [/h3]

[list]
  [*] First public release.
[/list]
0 Kudos
Reply
3 Replies

1,115 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Feb 23 02:35:57 MST 2016
Latest release now v1.7.0 build 696, 23 Feb 2016
0 Kudos
Reply

1,115 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Thu Nov 26 03:11:33 MST 2015
Latest release now v1.6.0 build 652, 26 Nov 2015
0 Kudos
Reply

1,115 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Tue Jun 23 09:17:58 MST 2015
Latest release now v1.5.2 build 588, 23 June 2015
0 Kudos
Reply