LPCLink 2 supported targets

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCLink 2 supported targets

1,152件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by miccio on Fri May 20 02:19:17 MST 2016
Hello my fellow LPC users,

A bit of a heretic question for you: has anyone tried to use LPCLink2 debuggers (either stand-alone or embedded in some LPCXpresso v2+ eval. board) with 3rd party targets?
Not bailing out on LPC, but we just got an STM-based design from an external collaborator with 2x5 swd pin headers and the only debuggers around with such footprints are the LPC ones.

Thanks in advance.
0 件の賞賛
返信
3 返答(返信)

1,131件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

1,131件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by miccio on Fri May 20 03:33:37 MST 2016
thanks for the prompt answer vtw.433e,

I was just afraid that either of the manufacturers would have put in place some kind of restriction.

Have a nice weekend!
0 件の賞賛
返信

1,131件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Fri May 20 02:30:02 MST 2016
Load it with CMSIS-DAP firmware and it will work with any ARM target - from a debugger all ARM targets look pretty much the same.

BTW: You can buy an adapter to convert the traditional JTAG connector to the small SWD-style connector, so you can use your other adapters too. I know the Embedded Artists do one, but lots of other do too.
0 件の賞賛
返信