LPCExpresso install on USB thumb drive

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCExpresso install on USB thumb drive

1,053 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Tue Dec 09 17:00:57 MST 2014
I am wondering whether or not LPCExpresso and LPCOpen and workspaces can all be installed on a thumb driver.
the goal is to have a complete portable development environment.
So the real question is how much junk does Eclipse and other packages place in the registry?
0 项奖励
回复
3 回复数

1,046 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Wed Dec 10 16:50:08 MST 2014
thanks, I'll try it and see.
slow does not matter as much as the convenience of take-it-anywhere.
And I really just want to write and compile code.  I can debug on my main dev PC.
I can sync up source code from a solution folder to my main development PC when I make changes.
0 项奖励
回复

1,046 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Wed Dec 10 02:11:59 MST 2014
When it was Code Red, they said that it did not use any registry.

However, the licence file(s?) goes in "Documents and Settings"/"User" <yourname>/something
And debugging etc. runs scripts that need a windows "cscript?" somewhere on the path.
Also USB device drivers are installed (on the PC) at installation.

So probably not.

Also, Java bloatware is huge so you would need a big memory stick.
My 7.4 installation on Win7-64 is 741 megabytes. That's without the workspaces.

Mike
0 项奖励
回复

1,046 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Dec 10 02:09:50 MST 2014
LPCXpresso does not use the Registry directly (although the installer does place some install/uninstall information there, it is not used by the product when running).

We have not tried it, but I don't see any reason why it should not work, subject to the following caveats:
- If you want to debug, drivers for USB debug adapters will need to be installed on each machine. They can be found in the Drivers directory of the install directory
- Any target machine will need the Visual Studio redistributables installed. Many machines have these installed, but if not, you need to run the vcredist_x86.exe installer found in the install directory
- Performance is likely to be slow. The IDE uses its install directory to cache a lot of (run time) information. USB flash drives are typically very slow for this sort of information
- There is some configuration information stored in the "configuration" (!) directory. Some of this includes path information, including the drive letter. I don't expect this to cause any significant problems
- Workspaces are not designed to be portable like this. They will contain full paths that are likely to cause issues when moving between machines of the USB flash drive has a different drive letter (i.e E: or F:). However, you can normally recover this by using File->Import, General/Existing projects into workspace

There may be others, but these are the ones that I can think of immediately. All I can suggest is - try it and report back your findings. Good luck.
0 项奖励
回复