LPCExpresso 1769 LCD help required

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCExpresso 1769 LCD help required

3,320件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alexantosh on Sun Feb 10 13:32:03 MST 2013
hi everyone;
i just got my lcpexpresso 1769 and connected it successfully to a board and pc. everything works fine so far, but i cant get the LCD to display any text or anything.
i have gone through the forums but have seen nothing of the sort. any sample code - however simple will be appreciated - if not against the rules that is.
Thanks
0 件の賞賛
返信
17 返答(返信)

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alexantosh on Mon Feb 11 11:55:23 MST 2013
alright then.:(
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alexantosh on Mon Feb 11 11:54:50 MST 2013
alright.
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Feb 11 11:34:44 MST 2013

Quote: alexantosh
so in short u r suggesting that i just throw this board away and getting something better right:rolleyes:??



If you are free to choose a display I would suggest that. A nice TFT is much more impressive than an old-fashioned 2*16 LCD. And the time you spent with it's software isn't wasted, it's a real eye-catcher :)


Quote: alexantosh
btw. can you point me to lpcexpresso samples that can work for this  time?



I'm not aware of any I2C LCD LPCXpresso project, sorry :(
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alexantosh on Mon Feb 11 11:18:46 MST 2013
so in short u r suggesting that i just throw this board away and getting something better right:rolleyes:??
btw. can you point me to lpcexpresso samples that can work for this time? am newbie to this thing but it is interesting. the other modules were fun till curiosity overrode all of them :(- the only thing that is on my mind now is seeing something from the screen:)!!
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Feb 11 08:19:47 MST 2013
I was surprised that a joker added a 10 year old I2C (400kHz) LCD display to a LPCXpresso1769. Looks like a sick joke to me :) Google showed this University board. I assume they also have examples for this display :confused: I would always suggest to use something faster (SPI) and more colored (TFT) with Touchscreen :rolleyes:

But anyway, I don't know what you are planning. Datasheet of display is describing how to use I2C display commands and LPCXpresso I2C examples are also available. Perhaps you can find a sample or you want to spent a lot of hours writing your own driver. If that's not an educational project I would just use something newer. A nice modern 320x240 TFT is looking very cool and easy to connect to a LPCXpresso via SPI :cool:
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alexantosh on Mon Feb 11 07:25:15 MST 2013
so do you know the board am talking about :) or did you just trace that url using the board number i gave you? 'coz he really beamed it up.
if so, is there a way i can display text on the screen? :confused:
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Feb 11 05:34:01 MST 2013

Quote: alexantosh
:eek:Then Scotty beamed it up for me for sure. do you know him personally or are you a friend of his:)!?!



Unfortunately not :( But every time something strange happens, I'm trying to blame him (or E.T.) ;)
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alexantosh on Mon Feb 11 05:13:16 MST 2013
:eek:Then Scotty beamed it up for me for sure. do you know him personally or are you a friend of his:)!?!
am in istanbul too.
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Feb 10 15:37:18 MST 2013
Scotty is in Istanbul :)

http://www.fatih.edu.tr/~ifyalciner/index.html
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alexantosh on Sun Feb 10 15:01:40 MST 2013
@wrigh ; no it's not that board.
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alexantosh on Sun Feb 10 14:57:12 MST 2013
ok, let me try it out. but right now i have gotta go somewhere. i will let you know tomorrow. thanks alot. am gonna try it out tonight!
- probably scotty did his thing though! :)
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wrighflyer on Sun Feb 10 14:50:11 MST 2013
Is it this board by any chance?

www.embeddedartists.com/products/lpcxpresso/xpr_base.php

That has an OLED display. EA's page says they have driver code for it. (oh and a user manual).
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Feb 10 14:44:42 MST 2013
http://www.newhavendisplay.com/specs/NHD-C0216CiZ-FSW-FBW-3V3.pdf  :confused:

Did you buy the board anywhere or did Scotty beam it up?
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alexantosh on Sun Feb 10 14:36:41 MST 2013
To be honest am not so sure about the specific name of the board am using  :eek:; but so far i know that it is the the lpcexpresso development board. nothing close to a name is written on it, but The model number of LCD Display is ‘NHD-C0216CiZ-FSW-FBW-3V3’:o. that is as much as i have scrapped now.
also in the documents i didnt see anything like the board's name but if there is anything specific that is required about it, then tell me it to me so that i can look for it :)
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Feb 10 14:17:25 MST 2013

Quote: alexantosh
@zero; the lcd is not on the lcpexpresso, it's on the board.



I see, it's a guessing game :)

So which board did you connect :confused:
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alexantosh on Sun Feb 10 14:00:25 MST 2013
@zero; the lcd is not on the lcpexpresso, it's on the board.
0 件の賞賛
返信

3,264件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Feb 10 13:48:44 MST 2013
:confused:

My LPCXpresso1769 has no LCD, so what LCD did you connect?
0 件の賞賛
返信