LPC4337 M4 debug problem if M0 program is before M4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4337 M4 debug problem if M0 program is before M4

Jump to solution
2,296 Views
klatecki
Contributor I


Hi,

 

I have problem with debugging M4 program if M0 program is before M4. It's look like this:

154365_154365.pngpastedImage_5.png

 

Bootloader run M4 program from Flash B then M4 run M0 Program from Flash A.

Debugging M4 program in this configuration is impossible. It's look like debugger try run Cortex M0 as M4 program.

 

Debug Messages Logs:

 

LPCXpresso RedlinkMulti Driver v8.1 (Mar 11 2016 13:34:34 - crt_emu_cm_redlink build 672)

Found chip XML file in D:/Projekty/ISM/iSMASedona/Firmware_new/Sedona/Release/LPC4337.xml

Probe Firmware: LPC-LINK2 CMSIS-DAP V5.147 (NXP Semiconductors)

Serial Number:  CWG2CUCV

VID:PID:  1FC9:0090

USB Path: \\?\hid#vid_1fc9&pid_0090&mi_00#8&2f6b45be&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}

Emu(0): Connected&Reset. DpID: 4BA00477. CpuID: 410FC240. Info: <None>

Debug protocol: JTAG. RTCK: Disabled. Vector catch: Disabled.

inspected v.2 On-chip Flash Memory C:\nxp\LPCXpresso_8.1.4_606\lpcxpresso\bin\Flash\LPC18x7_43x7_2x512_BootA.cfx

image 'LPC18x7/LPC43x7 2x512KB (Boot Bank A) Feb 16 2016 09:18:47'

NXP: LPC4337  Part ID: 0x00000000

Connected: was_reset=true. was_stopped=false

LPCXpresso Free License - Download limit is 256K

Writing 9292 bytes to address 0x1A010000 in Flash

Erased/Wrote page  8-8 with 9292 bytes in 230msec

Flash Write Done

Writing 220916 bytes to address 0x1B000000 in Flash

Erased/Wrote page  15-25 with 220916 bytes in 2446msec

Flash Write Done

Flash Program Summary: 230208 bytes in 2.68 seconds (84.01 KB/sec)

============= SCRIPT: LPC18LPC43InternalFLASHBootResetscript.scp =============

Boot from FLASH image pc/sp reset script

PC = 0x1A011641

SP = 0x20010000

XPSR = 0x01000000

VTOR = 0x00000000

============= END SCRIPT =====================================================

 

 

If M0 program is after M4 program then everything works well.

How to debug M4 program in this configuration as above?

Labels (1)
0 Kudos
Reply
1 Solution
2,069 Views
klatecki
Contributor I

Hi,

thank you for quick reply.

I dont' download the bootloader with the application.

I added this line to the script:

101 a% = peek32 this 0x1b000004

and its works!

Thank you a lot!

View solution in original post

0 Kudos
Reply
2 Replies
2,069 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Do you download the bootloader along with the application code? If so, you could modify the LPC18LPC43InternalFlashBootResetScript.scp to provide the bootloader entry as the initial PC, then deal with stopping execution in the M4 code. Doing this might make sense if the application relies on something in your bootloader setup, but it's somewhat messy to do. If you don't download the bootloader with the application (the more common case), then modify the script PC setting to use the M4 entry, not the M0 entry as it appears now.

Thanks and regards,

LPCXpresso Support

0 Kudos
Reply
2,070 Views
klatecki
Contributor I

Hi,

thank you for quick reply.

I dont' download the bootloader with the application.

I added this line to the script:

101 a% = peek32 this 0x1b000004

and its works!

Thank you a lot!

0 Kudos
Reply