LPC4322 board detection on Ubuntu 12.04.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4322 board detection on Ubuntu 12.04.

352 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mbilal on Mon Oct 27 10:51:06 MST 2014
Hi,

I have LPC 4322 expresso v2 board.
I downlaoded the CMSIS-DAP image for using the on-chip debuger by using the LPC configuration tool.
I can see the CMSIS-DAP debugger option on Windows host easily by using Sourcery CodeBench debug Sprite.
But I'm not seeing the CMSIS-DAP option on UBUNTU 12.04 (32 bit) host by using the Sourcery CodeBench debug Sprite.

I think it is LPCexpresso device detection failure on Linux machine.
I have updated the udev rules with 85-lpcexpresso.rules but doesn't work.

Am I missing something to be able to detect the LPC4322 on Linux machine?

Could you please help me on this regard?


Thanks,
-Bilal
0 Kudos
Reply
1 Reply

334 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed Oct 29 04:36:08 MST 2014
Suggest that you ask CodeSourcery why it is not supported on Linux.

Note that this works correctly with LPCXpresso.
0 Kudos
Reply