LPC4088 Segger EMWIN Compatibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC4088 Segger EMWIN Compatibility

722 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by paul.rcom-software.com on Thu Jul 24 14:30:33 MST 2014
I am using an Embedded Artists LPC4088-32 dev. board with the Rowley Crossworks toolchain and
LPCXpresso.  Does anybody know if the EMWIN graphics package has been successfully ported
to this environment--or a close one ?

This is the information about the graphics hardware I plan to use.

* On-Board LCD Controller

LCD controller, supporting both Super-Twisted Nematic (STN) and Thin-Film
Transistor (TFT) displays.

- Dedicated DMA controller.

- Selectable display resolution (up to 1024 × 768 pixels)

Selectable display resolution (up to 1024 × 768 pixels)

Features and capabilities are detailed in chapter 11 of the NXP  UM10562 LPC407X/408X User Manual.

NOTES: To be used in conjuction with a Kyocera 3 1/2" QVGA LCD display--model
number T-55343GD035JU-LW-ADN

Best Regards,

Paul R.
0 Kudos
Reply
1 Reply

698 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Jul 25 00:12:25 MST 2014
LPCOpen is available for EA's LPC 4088 Developer's Kit board from

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc40xx-packages

and emWin for LPC MCUs is available from:

http://www.lpcware.com/content/project/emwin-graphics-library

I would also advise checking the EA website pages for the board - http://www.embeddedartists.com/products/kits/lpc4088_kit.php

Regards,
LPCXpresso Support
0 Kudos
Reply