LPC18S37 SPIFI flash driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC18S37 SPIFI flash driver

1,108件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pggordini on Wed May 27 06:17:12 MST 2015
I try an OM13076 board _ LPC18S37 but LPCxpresso do not find the required flash driver.
Where can I find to add to LPCxpresso ?

Yours Sincerely,

Pier Giovanni

0 件の賞賛
返信
3 返答(返信)

1,075件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri May 29 11:00:12 MST 2015
An LPCOpen bundle for the LPCXpresso18S37 board has recently been released at:

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc18xx-packages-0

Regards,
LPCXpresso Support

0 件の賞賛
返信

1,075件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pggordini on Fri May 29 04:00:20 MST 2015
I am new to ARM and LCPXpresso, so probably i have started in the wrong way.
I have searched for a file for 18S37, but i have found only a collection generic 1800.
The selected file may be for an MCU whith different memory lay-out so the problem.
May I find a file to test my tool chain with the OM13076 board that can be compiled and debugged without
any intervention ?

Best Regards,

Pier Giovanni

0 件の賞賛
返信

1,075件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Wed May 27 09:30:16 MST 2015
For a project configured for LPC18S37, the LPCXpresso IDE will default to using the internal flash and flash driver.

If you want to configure to use external SPIFI, you will need to modify the memory configuration (as detailed in the LPCXpresso User Guide) and select the appropriate flash driver - as per http://www.lpcware.com/content/faq/lpcxpresso/lpc18-lpc43-spifi-flash-drivers

If you want to boot from SPIFI, note that you will need to modify the boot jumpers and also ensure that the internal flash is mass erased.

[You might also want to take a look at the LPCScrypt tool - http://www.lpcware.com/lpcscrypt ]

Regards,
LPCXpresso Support

0 件の賞賛
返信