LPC17xx MCPWM register missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC17xx MCPWM register missing

1,125件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by martinho on Wed Apr 20 06:20:17 MST 2011
I'm missing the MCPWM Registers (Motor Control PWM) in the Peripherals view, I know i can watch directly the memory at 0x400B800, but this is not very intuitive to use. Would it be possible to add this in the next release?

Edit: Strangely the access seems not to work neither for the MCPWM not for the QEI peripherals (I hope they are present on my chip (LPC1752), I did not find any hint that they are present only on some chip's).

Edit Edit: I had disabled the QEI and MCPWM modules, for this reason i got errors when trying to monitor the Address 0d 0x400B800, this is now working, remains the problem with the missing MCPWM in the Peripherals view.

Martin
0 件の賞賛
返信
3 返答(返信)

1,066件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by martinho on Wed Apr 20 10:45:49 MST 2011

Quote: larryvc
I have reported this to CodeRed Support.

Larry



Thank's a lot Larry!

Martin
0 件の賞賛
返信

1,066件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Wed Apr 20 10:13:45 MST 2011
I have reported this to CodeRed Support.

Larry
0 件の賞賛
返信

1,066件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Polux rsv on Wed Apr 20 07:51:09 MST 2011
Reads the errata sheets. I remember something is not working for motor control on one or more LPC17xx devices.

Angelo
0 件の賞賛
返信