LPC1788 Develop Kit + IAR Jlink lite + LPCXpresso 4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788 Develop Kit + IAR Jlink lite + LPCXpresso 4

906 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Blogs on Wed May 23 22:24:02 MST 2012
Hi there,

I would like to know if it is possible to use the IAR Jlink lite to flash my LPC1788 through LPCXpresso 4 debug tool?

I have tried building it, however the program cannot see the Jlink tool.

However it seems the board recognises the Jlink lite connection, since when I plug it in, it restarts the on demo program.

Thanks.
0 项奖励
回复
2 回复数

864 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Tue May 29 02:41:43 MST 2012

Quote: NXP_Europe

The LPCXpresso IDE can only work with the LPC-link as debugger, there is no support for other debuggers.


Incorrect : see http://www.code-red-tech.com/products.php#comparison

But in summary, the LPCXpresso IDE can work with the following debug probes:
- LPC-Link
- Red Probe / Red Probe+
- RDB1768 (probe built into board)

And to answer the original question explicitly - it will not work with Jlink.

Regards,
CodeRedSupport
0 项奖励
回复

864 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Tue May 29 02:34:03 MST 2012
Hi,

The LPCXpresso IDE can only work with the LPC-link as debugger, there is no support for other debuggers.

The reset you're seeing is just due to a glitch on the reset pin caused by the Jlink.

Regards,
0 项奖励
回复