LPC1769 error reported

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1769 error reported

3,527 Views
sebastianbarcia
Contributor I

Hierror.jpg

I was debugging a project of lpc1769 with lpcxpresso and show me the follow code error. Is the microcontroller dead?
How can i fix it?
Thanks

0 Kudos
Reply
3 Replies

3,258 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Have you ever been able to debug your system? If so what changed, or what code did you program into the MCU, before it stopped working?

Is this an off-the-shelf board, or your own board? 

If your own board, please check out - https://community.nxp.com/message/630601 

What debug probe are you using?

What version of LPCXpresso IDE are you using? And on what host OS ?

Please also double check that you following the process for booting the chip into ISP mode correctly - you must be pulling the ISP pin as the board is reset/powered up.

Regards,

LPCXpresso Support

0 Kudos
Reply

3,258 Views
lpcxpresso_supp
NXP Employee
NXP Employee

In the first place, see :https://community.nxp.com/message/630748 

Regards,

LPCXpresso Support

3,258 Views
sebastianbarcia
Contributor I

Thanks for your reply
None of that worked
I can not erase the flash

Mode ISP not response

0 Kudos
Reply