LPC1769 Rev A / Rev B

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1769 Rev A / Rev B

3,445 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bobi-one on Mon Jun 13 08:53:33 MST 2011
It seems i cannot find  lpcxpresso with LPC1769 in Bulgaria. However there was some company that offers unknown LPC17xx veriosn of the board. Are the difference in the board significant, and is there some official distributor for NXP.
0 项奖励
回复
12 回复数

3,389 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Tue Jun 14 22:52:07 MST 2011
Luis, Bobi,

this thread is bout the lpc1768/69 LPCXpresso board, not the 11u14.
Mixing in other questions that have nothing to do with the original question might confuse the originator of this thread (ehhh... being... :D)

For this once: [I]read[/I]  the Embedded Artists website (I've been looking at the photo too long and almost missed it).
Below the photo of [I]an[/I] LPCXpresso board it reads:

Quote:
Picture not showing correct version of LPCXpresso board.                                                              

and in the product specifications:

Quote:

[I]Connectors[/I]
                                                • mini-B USB connector for LPC11U14 USB interface
                                                     • All LPC11U14 pins available on expansion connector (2x27 pin rows, 100 mil pitch, 900 mil between rows)

I think I now also understand what Luis means with

Quote:
Remember to use the lenses for the fine print.:)



Rob
0 项奖励
回复

3,389 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Tue Jun 14 15:07:38 MST 2011
That picture shows LPC1114 :)

And below this picture you can read:

"Picture not showing correct version of LPCXpresso board."
0 项奖励
回复

3,389 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Tue Jun 14 15:06:40 MST 2011

Quote: bobi-one
I dont see extra usb on this boart




Quote:
Picture not showing correct version of LPCXpresso board.



Remember to use the lenses for the fine print.:)
0 项奖励
回复

3,389 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bobi-one on Tue Jun 14 14:59:34 MST 2011

Quote: Luis Digital
[B]LPC11U14 LPCXpresso Board[/B]


I dont see extra usb on this boart
0 项奖励
回复

3,388 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Luis Digital on Tue Jun 14 14:31:01 MST 2011

Quote: bobi-one
BTW do somebody know what is this LPCxpresso (if it is xpresso)
http://www.youtube.com/watch?v=A2FiHiTNlY4  it looks like something new. The extra usb port looks really neat



[B]LPC11U14 LPCXpresso Board[/B]
0 项奖励
回复

3,388 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bobi-one on Tue Jun 14 11:42:18 MST 2011
BTW do somebody know what is this LPCxpresso (if it is xpresso)
http://www.youtube.com/watch?v=A2FiHiTNlY4  it looks like something new. The extra usb port looks really neat
0 项奖励
回复

3,388 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Tue Jun 14 05:58:23 MST 2011
"not vibration proof"???

From the datasheet of one of those type of crystals (I found that other crystals have similar specs):


Quote:
MAXIMUM 75 cm DROP TEST IN 3 AXES ONTO A HARD SURFACE
OR 3000 g x 0.3 ms x ½ SINEWAVE IN 3 AXES

it is wise to fix the crystal in place instead of letting it float on its wires but the crystal withstands most vibrations without a problem.

Rob
0 项奖励
回复

3,388 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Polux rsv on Tue Jun 14 02:09:30 MST 2011
Rev B has a smd 32kHz crystal instead of the "not vibration proof" one.

Angelo
0 项奖励
回复

3,388 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Rob65 on Mon Jun 13 12:19:19 MST 2011
The differences between the board are minimal.
The old board has an lpc1768 and a 24aa256 (256 kBit EEPROM) whereas the new board has an lpc1769 and a 24aa64 (64 kBit EEPROM).
RevA and RevB apply to the schematics and boards only, this is not linked to the revision of the lpc17xx chip used.

Please note that Embedded Artists does not guarantee that a certain revision of a chip is being used. According to their FAQ:


Quote:
We do not sell a specific chip revision. Normally it is the latest, but  when new revisions are released by NXP there can be a transition period.

If a local vendor stocks chips or boards these could still be old versions.
I've read that somebody just bought a board which still had the R- revision of the chip (the worst bug in the R- version is the RTC problem).
I just bought a batch of lpc1754 chips from Farnell and (YES!) these have an RA marking so RTC works:)

Rob
0 项奖励
回复

3,388 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Jun 13 10:05:01 MST 2011
Don't know the differences :), but I think you can't buy a (new) LPCXpresso1768 today. It was sold out for month and then LPCXpresso1769 was sold and is now actual stock product.

http://www.embeddedartists.com/products/lpcxpresso/lpc1769_xpr.php?tab=res
0 项奖励
回复

3,388 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bobi-one on Mon Jun 13 09:52:54 MST 2011
I use intermediate company when buy from farnell, and they wasn't very sure, what kind of Xpresso is the one ( the only 17xx ) board at the site.
BTW: is the difference between rev A and B board the microcontroller, or there are twho types of LPCXpresso , with LPC1768 and 1769?
0 项奖励
回复

3,388 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Mon Jun 13 08:57:39 MST 2011
Distributor:

http://www.nxp.com/profile/sales/europe_dist/#bul

or Farnell

http://bg.farnell.com/

Note: Although you can find a LPCXpresso1768 at Farnell, they sell the new LPC1769 version.
0 项奖励
回复