LPC1769 Project From Template

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1769 Project From Template

904 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by furkan.yuksel on Thu Jun 23 07:09:55 MST 2011
Hi,

I'm using both LPC1114 and LPC1769 boards and I created project for LPC1114 with using smat import mode. However, I couldn't find similiar way for LPC1769, are there any template for LPC1769 as in 1114?
0 Kudos
Reply
1 Reply

788 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Europe on Fri Jul 08 05:50:24 MST 2011
If you install the latest LPCXpresso v4, you can select templates for a wide variety of families, including the LPC1769. In the ‘Quick’ tab select ‘New project’. Then select ‘NXP LPC1700 projects’

  You can also start by importing sample projects. In the ‘Quick’ tab, select ‘Import and Export’. Then ‘Import archived projects (zip). Select example projects from the LPCXpresso installation folder. The default location is: C:\nxp\LPCXpresso_4.0.5_123\lpcxpresso\Examples\NXP\LPC1000\LPC17xx
0 Kudos
Reply