LPC1766 Sample Program

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1766 Sample Program

1,917 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mahalinr on Thu Sep 11 05:56:28 MST 2014
Hallo

          I want to use LPC1766 Microcontroller. in my project.


Can anyone send me a sample program of LPC1766 CAN Communication.



Thanks in advance
0 项奖励
回复
5 回复数

1,883 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mahalinr on Tue Oct 07 05:08:12 MST 2014
How to implement CAN Communciation between LPC1766 and LPC11C24.


If you have any sample codings,please post it here


Thanks
0 项奖励
回复

1,883 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mahalinr on Sun Sep 14 23:12:40 MST 2014
Ok thankyou
0 项奖励
回复

1,883 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Sun Sep 14 19:52:14 MST 2014

Quote: mahalinr
The above link displays several files and in that for flashing the program and reading the adc which option should I choose?



Wild guess: a project with adc in its name...
0 项奖励
回复

1,883 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mahalinr on Sun Sep 14 14:11:34 MST 2014
Thanks

                          The above link displays several files and in that for flashing the program and reading the adc which option should I choose?

a) Freertos

b) Peripherals

c) lwip

d)misc

Plz let me which one should I chose for flashing my program and read  the ADC values
0 项奖励
回复

1,883 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Sep 12 03:21:07 MST 2014
As a starting point look at the example in the LPCOpen bundle for the LPCXpresso1769 board…

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc17xx-packages

You could also try doing a forum search for "LPC17 CAN" or similar to find previous threads.

Regards,
LPCXpresso Support
0 项奖励
回复