LPC1765 Debug Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1765 Debug Issue

1,050件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by corwin on Thu Dec 23 14:42:03 MST 2010
Hello,

I'm having an issue while trying to flash a program to the LPC1765. Here is the error message LPCXpresso gives me:

Error launching Debug\Sample.axf
02: Failed to connect: Em(12). System rejected access at location
0xE000EDF0 - verify population of memory and peripherals.

I have verified that my memory map is correct (I am using the default for LPC1765)

Thank you for help,
0 件の賞賛
返信
2 返答(返信)

1,040件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Steve Evans on Thu May 12 12:05:03 MST 2011
Was this issue resolved?

Steve
0 件の賞賛
返信

1,040件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Dec 23 15:26:53 MST 2010
In the first place, please read the below FAQ - plus the FAQ's that this links to:

http://support.code-red-tech.com/CodeRedWiki/FailedToConnect

I suspect that you have managed to program some code into the flash of your board that has destabilized the system - and booting into the ISP will allow you to recover things.

Regards,
CodeRedSupport
0 件の賞賛
返信