LPC1764 SRAM Allocation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1764 SRAM Allocation

1,439件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by djtilava on Fri May 27 21:16:04 MST 2016
I am using LPC1764 with LPC xpresso IDE 8.1.0_597 for making Serial to ethernet converter. In LPC1764 there are two sections of SRAM. My question is that HOW can i use second SRAM (from Mem location 0x20000000)?? Whether it is automatically access when local SRAm is full or we have to pointed to AHB SRAM to access it? Or how can i directly put my variables in AHB ram during Run time?
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,315件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

1,315件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun May 29 03:16:23 MST 2016
See:

Only the first block of RAM will be used by default. There are various ways of using the second. For more information see:

[list]
  [*]https://www.lpcware.com/content/faq/lpcxpresso/data-different-ram-blocks
  [*]https://www.lpcware.com/content/faq/lpcxpresso/heap-checking-redlib
  [*]https://www.lpcware.com/content/faq/lpcxpresso/freemarker-linker-script-templates
[/list]

Regards,
LPCXpresso Support
0 件の賞賛
返信