LPC15xx Attach only Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC15xx Attach only Problem

2,328件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by R2D2 on Sat May 09 12:40:37 MST 2015
As usual I'm trying to debug a running system with 'Attach only'...

Unfortunately that's not working with my LPC1549 / LPC-link2 / Win8.1 / LPCXpresso v7.7.2 [Build 379] [2015-03-31]   :((

[img=809x284]http://www.lpcware.com/system/files/Attach.JPG[/img]

Looks like 'Attach only' isn't overwriting 'Load Image'  :quest:

After setting 'Load Image' false, Attach only is working...
0 件の賞賛
返信
3 返答(返信)

2,221件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Mon May 11 00:49:28 MST 2015
We have reproduced the problem, and are investigating. Thanks for reporting.
0 件の賞賛
返信

2,221件の閲覧回数
juanabelaira
Contributor III

Still researching after two years?

0 件の賞賛
返信

2,221件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

I'm not sure what you are suggesting - but IIRC the issue described here was fixed in the next LPCXpresso IDE release, a month or so after this thread was created.

If you are having problems with attach yourself, I would suggest creating a new forum thread, and posting full details - including what MCU you are using and what version of LPCXpresso IDE (or MCUXpresso IDE) you are using.

Regards,

LPCXpresso Support

0 件の賞賛
返信