LPC13xx EE_Write from flash source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC13xx EE_Write from flash source

757 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by efiLabs on Fri Aug 30 22:57:49 MST 2013
friends :

tried to write to the ee-mem using iap function pointer calls

everything seems to work just fine ...

except if you want to copy bytes from flash to ee-mem

1st it seems to return error code 14, which is not an iap error code, it could be an isp code

14 ADDR_NOT_MAPPED
Address is not mapped in the memory map. Count
value is taken in to consideration where applicable.

the IAP Status Codes end at 11

any particular reason why i wouldn't be able to read the data for my ee-mem writes from flash ??? like some inits ???

either i'm dreaming or who ever wrote the boot code and or the user manual.

sorry for my comments, but i spent considerable code chasing my tail this way.

at least that's the way it looks for me right now.

anyone with similar experiences ??? please step forward and share it with us :)

thanks and cheers efiLabs

0 Kudos
Reply
1 Reply

728 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by efiLabs on Sat Aug 31 00:20:10 MST 2013
ok i read through the user manual again and it says RAM addr for both, EE_Rd and EE_Wr

doesn't make sense to me to restrict the EE_Wr to RAM alone ... now i have to copy the Flash based init data 1st to RAM and then to EE-mem ... what a waste

cheers, efiLabs

p.s. the wrong error code 14 is still not resolved
0 Kudos
Reply