LPC13xx Composite Device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC13xx Composite Device

528件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jush on Fri Apr 01 01:48:49 MST 2011
Hi,

I run the example about creating a composite device of USB, it is about MSC and CDC combination.
I want to create a composite device using HID ROM and MSC ROM.It is possible to combine this two (using on-chip ROM)?I already do like as describe in  the document but still when i run the project it didn't enumerate the MSC and HID.:confused:
Someone could help me about this?

Thanks.
0 件の賞賛
返信
0 返答(返信)