LPC1347 watchdog problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1347 watchdog problem

492件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Marcus on Sun Feb 24 10:03:00 MST 2013
Hello,

I have the following problem with the watchdog feature of the LPC1347.
When I program the WDMOD register with 0x0023, all works as expected.
But when I set it to 0x0033 (with the WDPROTECT bit active), the watchdog does not react to a hangup test at all.  As I understand, WDPROTECT protects the TC register against unintentional changes, but the TC register was already set befóre writing WDMOD. Any help or suggestions would be fabulous.

Marcus.
0 件の賞賛
返信
0 返答(返信)